Award-winning solutions from Belden, Grass Valley and SAM come
together for in-person, live product demonstrations
ST. LOUIS--(BUSINESS WIRE)--
Belden Inc. (NYSE: BDC), a global leader in signal transmission
solutions for mission-critical applications, is excited to showcase its
award-winning, behind-the-scenes connectivity solutions – which brings
media and entertainment technology to life – at NAB on April 9-12, 2018,
in Las Vegas.
Visitors to Booth SL106 will see unified solutions available from the
Belden, Gepco, Grass Valley and ex-Snell Advanced Media (SAM)
portfolios; in-person, live demonstrations will illustrate how these
solutions support news, live production, networking and content delivery
applications.
NAB marks the debut of the combined product portfolios of Grass Valley
and SAM, offering customers the largest selection of broadcast
technology backed by unmatched R&D resources and the superior financial
stability of Belden. Grass Valley will be showing its solutions for live
production, news, content delivery and networking, with a focus on
virtualization, IP and HDR.
In addition to the Grass Valley demonstrations, attendees will also be
able to experience the following Belden branded products in action:
-
4K UHD Coax Cables and Connectors for 12G-SDI, an award-winning
solution that maximizes 4K signal transmission over a single coax
while minimizing space and weight.
-
4K UHD Media Cable, another award-winning innovation, which is
certified for HDBaseT applications and delivers 4K content over 100 m
with a cable that’s smaller and lighter (and can be combined with
REVConnect).
-
Custom Broadcast Assemblies that are built to length, custom
configured and rigorously tested (with accompanying performance
reports), and can be terminated with a wide variety of connectors.
-
Broadcast Panels in both standard Gepco branded and custom
configurations designed and engineered to meet the unique requirements
of studios, live production and large venue applications.
-
Custom Fiber Panels that can be loaded with connectors or left
blank, in a variety of configurations: flat, flanged or chassis. The
panel’s connector punches can be made for a complete range of
broadcast and pro AV connector formats.
-
FiberExpress Fusion Splice-On Connector, which combines
the benefits of fusion splicing with the simplicity of
field-installable connectors while eliminating the need for splice
enclosures and trays.
-
FiberExpress ECX Patch Panel – which has also received
industry recognition for product innovation – makes installation in
tight spaces easy, eliminates fiber pinch points and supports fast
moves, adds and changes.
-
REVConnect Connectivity System, which creates a reliable,
gas-tight connection while reducing rework, requiring less time for
termination and supporting all category cables with one termination
method. Since its release in late 2016, REVConnect has been recognized
five times for product innovation.
NAB attendees should also make sure to visit Thinklogical at Booth
SL6328, another Belden brand and worldwide leading designer and
manufacturer of video and KVM signal extension and switching systems for
a wide range of broadcast and post-production applications.
For more information about Belden’s participation in NAB, visit www.belden.com/nab.
Only Belden’s innovative enterprise connectivity solutions take a
universal approach to customers’ enterprises, resolving signal
transmission needs with IP- and legacy-based solutions that enable a
smooth migration to convergence. Belden’s extensive portfolio spans LAN,
data centers, building automation and security and access control to
keep information running smoothly. Outstanding global service and
support capabilities and application-specific warranty programs complete
Belden’s unique offering.
About Belden
Belden Inc., a global leader in high-quality,
end-to-end signal transmission solutions, delivers a comprehensive
product portfolio designed to meet the mission-critical network
infrastructure needs of industrial, enterprise and broadcast markets.
With innovative solutions targeted at reliable and secure transmission
of rapidly growing amounts of data, audio and video needed for today’s
applications, Belden is at the center of the global transformation to a
connected world. Founded in 1902, the company is headquartered in St.
Louis and has manufacturing capabilities in North and South America,
Europe and Asia. For more information, visit us at www.belden.com;
follow us on Twitter @BeldenInc.
Belden, Belden Sending All The Right Signals, and the Belden logo are
trademarks or registered trademarks of Belden Inc. or its affiliated
companies in the United States and other jurisdictions. Belden and other
parties may also have trademark rights in other terms used herein.
View source version on businesswire.com:
https://www.businesswire.com/news/home/20180330005018/en/
Belden Inc.
Melissa Knapp, 937-336-5258
Media Relations
Melissa.Knapp@Belden.com
Source: Belden Inc.