Belden Expands Portfolio of Versatile Automation Tools to Meet Increasing IIoT Connectivity Demands

January 18, 2018

Enhancements to Lumberg Automation LioN-Power Family Streamlines Path to Fieldbus-Independent and One-Device Automation

ST. LOUIS--(BUSINESS WIRE)-- Belden Inc., a global leader in signal transmission solutions for mission critical applications, has expanded the Lumberg Automation LioN-Power product family to help industrial manufacturers address exploding Industrial Internet of Things (IIoT) connectivity needs through simplified device automation. The updates and additions bring added flexibility through universal digital I/O modules, as well as holistic solutions through new IO-Link system devices.

“Manufacturers need economical, straightforward ways to connect legacy systems and build out new networks. And they need the flexibility to manage a wide range of complex in-field automation and control tasks,” said Paul Just, product manager of I/O systems at Belden. “The updates to the LioN-Power family offer maximum versatility and cost-effectiveness. In addition to leveraging standardized protocols, the products feature user-friendly integration and configuration tools that eliminate the need for specialized programming skills.”

Enhancements to the LioN-Power product portfolio include:

  • The upgraded LioN-Power Multi-protocol I/O Modules take fieldbus-independent automation capabilities to the next level. The addition of 16 universal digital input/output (16DIO) channels, paired with cross-protocol functionality spanning PROFINET, EtherNet/IP and EtherCAT, make them the most versatile I/O modules on the market. Unique “Flex-Bit Technology” also makes connecting legacy machines with different bitmaps incredibly simple.
  • Lumberg Automation’s IO-Link System has expanded with the new LioN-Power IO-Link Hub with 16 digital inputs. Now, IO-Link devices, masters and hubs can be easily connected to efficiency process up to 132 I/O signals per system. With this solution, it makes financial and economic sense to upgrade from passive to active systems, or for distributed environments to collect many digital signals. Integration and configuration of IO-Link devices is also made effortless through the TMG IO-Link Device Tool.
  • The LioN-Power DCU1, the first multi-protocol distributed control unit with M12 power L-coding technology, now offers a 16DIO version. With UL 61010-1 approval, the LioN-Power 16DIO DCU can couple new and existing machines to an Ethernet network across PROFINET, EtherNet/IP and EtherCAT protocols – quickly transforming fieldbus machines into IP-ready devices. By delivering customized performance of automation functions within a single device, the DCU1 improves overall automation security and simplifies machine transparency.

All LioN-Power System components are designed to operate in the harsh and confined environments typical of robotics; machine and material handling; automotive and food/beverage manufacturing; transportation; and other industrial sectors.

For more information on the LioN-Power product family, visit https://www.belden.com/products/industrial/connectivity/io-systems.

In a world moving toward new levels of interoperability made possible by the Industrial Internet of Things (IIoT), visibility is vital to operators as they face increasing demands to receive, analyze and share data. Belden’s industrial connectivity solutions address these needs head on. With more connected machines, rising data volumes and increasing productivity demands, customers can count on Belden cable and Lumberg Automation and Hirschmann industrial connectors for a complete communications infrastructure designed to last. Belden’s customized systems provide high levels of performance and reliability to help a wide range of industrial automation applications handle the growth of intelligent, networked devices and robust analytics. Visit http://lumberg-automationusa.com to learn more.

About Belden

Belden Inc., a global leader in high quality, end-to-end signal transmission solutions, delivers a comprehensive product portfolio designed to meet the mission-critical network infrastructure needs of industrial, enterprise and broadcast markets. With innovative solutions targeted at reliable and secure transmission of rapidly growing amounts of data, audio and video needed for today's applications, Belden is at the center of the global transformation to a connected world. Founded in 1902, the company is headquartered in St. Louis and has manufacturing capabilities in North and South America, Europe and Asia. For more information, visit us at www.belden.com; follow us on Twitter: @BeldenInc.

Belden, Belden Sending All The Right Signals, Lumberg Automation, Hirschmann and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden and other parties may also have trademark rights in other terms used herein.

Source: Belden Inc.

Belden Inc.

Berry Medendorp, 31 77 387 8555

berry.medendorp@belden.com

or

Standing Partnership

Lindsay Auer, 314-287-6355

lauer@standingpartnership.com